{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there a way to make my ATV212 run a particular speed without a speed reference being given?
Issue:
Is there a way to make my ATV212 run a particular speed without a speed reference being given?

Product Line:
Altivar Machines, Altivar 212

Environment:
All

Cause:
Need to run the drive without a speed reference

Resolution:
Yes, set the drive's Lower Limit to the desired speed. The drive will run at that speed (assuming there are no conflicts with preset speeds or Upper Limit) when given a run command.

Schneider Electric Global