{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: What is the part number of the Expansion module to be used with TeSys T motor controller?
Issue:
Part number of the expansion module used in TeSys T

Product Line:
TeSys T

Environment:
LTMR

Resolution:
The part numbers are LTMEV40BD and LTMEV40FM. The expansion modules add voltage measurement between phases up to 690V nominal and 4 additional inputs.
  • LTMEV40BD: requires 24VDC input voltage with 4 inputs.
  • LTMEV40FM: requires 100-240VAC with 4 inputs.

Schneider Electric Global