{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to add plinth to Altivar Process ATV930C31N4F?
Floor standing drives ATV630 and ATV930, (ATVx30CxxF) are manufactured in Spacial SF enclosure.
Enclosure dimensions of ATV930C31N4F are 600mm (width) and 600mm (depth), height is 2150mm (2000mm enclosure + additional 150mm fan)
It is possible to add plinth and its references can be selected from Spacial catalog.
Full catalog downloadable from web (link below)
http://download.schneider-electric.com/files?p_Reference=9993CT0901&p_EnDocType=Catalog&p_File_Id=8636002994&p_File_Name=9993CT0901R08_16%20Body%20(Web).pdf

For ATV930C31N4F (and ATV630C31N4) it is possible to select plinth in 100mm or 200mm height. Find composition and references in attached extract from spacial catalog.

Schneider Electric Global

Attachment(s)
Extracted pages from Spacial F, 9993CT0901R08_16 Body (Web).pdf [155.36 KB]