{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the leakage currents for the sizes of the ATV12?
Issue:
Leakage currents for the sizes of the ATV12

Product Line:
Altivar 12

Environment:
All

Cause:
Documentation

Resolution:
Usually, the earth leakage current is defined from the unbalance voltage of 3% of the main
network for the three phase drives and maximum tolerance of RFI capacitors.
Here after find the leakage current:
leakage current

This leakage will be a function of other factors like motor cable, length motor cable, pwm
frequency, motor.

Schneider Electric Global