{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to run an ATV212 drive without a motor?
Issue:
Can the ATV212 drive run without a motor?

Product Line:
Altivar Machines, Altivar 212

Environment:
All models and serial numbers

Cause:
Run with no motor/load

Resolution:
Press Mode until you see AUF
Do not press Ent, arrow down to F- - -
Enter and arrow down to F605.
Set F605 to 0 to disable output phase loss.
You can now run the drive without a motor.

Remember to change F605 back to 1 to enable the output phase loss protection.

Schneider Electric Global