Browse FAQs

Are Power Monitoring Expert Activation IDs backwards compatible with previous versions?

Published date: 09 January 2020

Issue
The licenses sold are from the latest version of PME. 

Product Line
Power Monitoring Expert 2020
Power Monitoring Expert 9.0
Power Monitoring Expert 8.x


Environment
Activation IDs & PME Licensing

Resolution
The latest Activation IDs are backwards compatible from the latest version to PME 8.0 

Note: Older licenses do not work with the latest version. For example PME 9.0 licenses do no work in PME 2020.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.