Browse FAQs

On Ecostruxure Augmented Operator Advisor app, why my picture is badly displayed (wrong rotation or size) ?

Published date: 29 June 2020

Description

Exchangeable image file format (EXIF) is a standard that specifies the formats for images, sound, and ancillary tags used by digital cameras (including smartphones). All picture files include these metadata

A tablet read this hidden information to display the picture, but several picture editor don't overwritte the metadata and the tablet can display the picture as not expected on the Ecostruxure Augmented Operator Advisor 
app (AOA app).

For example, a subscene picture seems OK in the AOA builder but is displayed with a 90 degree rotation on AOA app.



Solution

To resolve this behavior you must edit picture with an editor to modify and save the correct picture's metadata then replace the picture on AOA builder with the correct image.


Product Familly
Ecostruxure Augmented Operator Advisor
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.