Browse FAQs

Can the Vijeo Design'Air Plus app be used with a SoMachine V4.3 / Vijeo Designer V6.2 application?

Published date: 16 December 2019

Issue:
Vijeo Design'Air Plus is not offered in Vijeo Designer that is integrated with SoMachine 4.3.

Product Line:
SoMachine, EcoStruxure Machine Expert

Resolution:
When using Vijeo Designer integrated with SoMachine or EcoStruxure Machine Expert, only the Vijeo Design'Air is available within a SoMachine V4.3 application. Vijeo Design'Air Plus is not supported.

Vijeo Design'Air is just direct virtual connection into the actual HMI Target. You will see exactly what is on the HMI with this app.

Vijeo Design'Air Plus is a different app. The smart phone or table is a second target in the HMI project. This Android / Iphone device cannot be added as a device from SoMachine.
Vijeo Design'Air Plus is only available with a standalone version of Vijeo Designer application.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.