Browse FAQs

Preventa XCS - what's happen if in daisy-chain of XCSRC RFID contactless safety switches (series model), the XCSRZE loopback device is not mounted?

Published date: 21 November 2019

 If in a daisy-chain of XCSRC RFID contactless safety switches (series model), the XCSRZE loopback device is not mounted on the last switch, the system detects a fault and the red led of the switch is continuously ON when the system is powered on. See attached pictures showing both cases; with or without the transpondeur. The red led can blink when the XCSRZE is removed from the system, machine on.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.