Browse FAQs

With only 3 inputs, can you use 2 preset speeds with the S-Flex Altivar 212?

Published date: 17 December 2019

Issue:
Can you use 2 preset speeds with the S-Flex Altivar 212?

Product Line:
Altivar ATV212 SFlex

Environment:
ALL

Cause:
Wiring / Programming

Resolution:


Press Mode to AUF (Quick Menu) Enter, set LL (Low Limit) to your 1st preset
Mode back to AUF - scroll down to F - - - (Extended Menu) and press Enter
F109 = 2
F118 = 6
Mode back to AUF, scroll down to
SR1.. Enter and set to your High Speed
Close P24 to VIA to run at high speed, open that contact to run at the LL - Low Speed setting
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.