Browse FAQs

Osisense XC - What is the XCMN2115L2L0 limit switch?

Published date: 19 October 2018

The XCMN2115L2L0 limit switch is an adapted limit switch, based on the XCMN2115L2 standard limit switch having head oriented 180° (L0 prefix meaning). See attached picture. Following part numbers exist too : XCMN2115L1L0, XCMN2115L3L0.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.