Browse FAQs

Osisense XC - Are the NC contacts of ZCKJ2 body complying with the positive opening operation?

Published date: 29 October 2018

The ZCKJ2 contacts are 2 CO simultaneous snap contacts. NC contacts are not complying with the positive opening operation (IEC 60947-5-1 Appendix K). Please refer to the attached picture

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.