What is the acceptable tolerance for the stripping length of a cable to be connected to the bare cable connectors of the Compact NSX?
For a correct installation of the wires to the bare cable connectors of Compact NSX, the cables must be stripped to the length indicated in the supplied instruction sheet, with the accepted tolerance of -0mm / +2mm.
Released for:Schneider Electric Global
Explore more
Range:
ComPact NSX
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.