{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Where do I connect my auto mode run command, on an enclosed ATS22 soft starter system?

Article available in these languages: Spanish

Issue:
Connecting Auto-Mode run command on an enclosed ATS22.

Product Line:
Enclosed ATS22 soft starter systems, part numbers beginning with 883922

Environment:
All enclosed ATS22 soft starter systems.

Cause:
Clarification of product features.

Resolution:
For Auto-mode run command on an ATS22 system, the run command will connect between terminals 5 and 6.  This will be a "2-wire" type connection where the motor will run as long as this connection is closed and will stop when this connection opens.

Schneider Electric Global