Browse FAQs

What EMC category does ATV320U55N4B-U75N4 comply?

Published date: 06 November 2018

ATV320...B meets the criteria of IEC61800-3 standards. However the EMC environment and categories can vary accoridng to motor cable length and existence of additional EMC filter.

ATV320U55N4B, ATV320U75N4B with integrated EMC filer (without additional filter) meets IEC 61800-3, category C3 with shielded motor cable up to 30m.
With additional filer VW3A4424 these drives will meet category C2 or C1 (100m in C3, 50m in C2, 10m in C1) shielded cable.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.