Browse FAQs

What is the replacement for the Magelis XBTGT1105 small touch panel HMI?

Published date: 26 November 2018

Issue

The Magelis XBTGT1105 small touch panel HMI is now a legacy product and is out of production. What is its replacement?


Product Line

Magelis small touch panel HMI, XBTGT1105, HMIGTO1300


Environment

Physical HMI

Resolution
The replacement for the XBTGT1105 (3.8" 320x240) small touch panel HMI is the HMIGTO1300 (3.5" 320x240) HMI.

Please see the following pages for comparison of the products:

 

XBTGT1105:

https://www.se.com/in/en/product/XBTGT1105/advanced-touchscreen-panel---320-x-240-pixels-qvga---3.8%22---24-v/

 

HMIGTO1300:

https://www.se.com/ww/en/product/HMIGTO1300/advanced-touchscreen-panel-320-x-240-pixels-qvga--3.5%22-tft---64-mb/

 

The dimensions for mounting in an enclosure are the same with the cosmetic front plate being 2 millimeters larger (on the outside of the enclosure).

The HMIGTO1300 also has an added a row of 6 function keys on the right of the screen.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.