Browse FAQs

What is the replacement for the legacy Magelis iPC MPCKT55NAX20N?

Published date: 26 November 2018

Issue

The Magelis iPC MPCKT55NAX20N is now a legacy product no longer in production. What is its replacement?

Product Line
Magelis iPC, MPCKT series Compact iPC


Environment

Physical Windows-based HMI


Resolution

The replacement for MPCKT55NAX20N is a combination of two parts:

 

The screen HMIDM7421:

https://www.se.com/ww/en/product/HMIDM7421/display-pc-4%3A3-15%22-single-touch-for-hmibm/

 

and the CPU/Motherboard box HMIBMUHI29D4801

https://www.se.com/ww/en/product/HMIBMUHI29D4801/modular-box-pc-hmibm-universal-hdd-dc-windows-10-4-slots/

 

 

The information page for the original MPCKT55NAX20N:

https://www.se.com/au/en/product/MPCKT55NAX20N/industrial-touchscreen-display---compact-ipc---15%27---intel-pentium-m-1.6-ghz/

 

On the above websites, please click on the "Dimensions Drawings" tab to review difference in the mounting solutions.

 

Please also see "MPCKT End of Life Instructions (ENVEOLI1404004EN_V1).pdf".

 

 

You may also want to consider these S-Panel PC one-piece panels:

https://www.se.com/ww/en/product-range/61054-magelis/791940132-panel-pc/?N=2005224983+48333542&Nr=AND%28product.siteId%3A700002%2COR%28product.catalogId%3Acatalog10007%29%29#tabs


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.