Browse FAQs

What are the technical specifications of the iPC with configured code HMIPCCP2NM7DA8K0KL00?

Published date: 26 November 2018

Issue

What are the technical specifications of the iPC with configured code HMIPCCP2NM7DA8K0KL00?

Product Line
Magelis iPC, Magelis Modular BoxPC Performance

Environment
Physical Magelis HMI

Resolution
HMIPCCP2NM7DA8K0KL00 is a configured Modular Box PC HMIBM Performance DC Base unit HMIBMP0I74DI00A plus the Magelis HMIDMA521 22" Wide Display (2 pieces together)
 
HMIPCCP2NM7DA8K0KL00 has the following attributes:
 
Form Factor: Modular Core i7 PC
Product Generation: Second Generation
Panel PC and Modular Display: Modular Display W22'' - FHD
Unit type:  Box PC Core i7 16GB-RAM, 2 PCI, Conformal coating (1xDP, 2xEth., 1xCOM, 4xUSB, MRAM)
CPU: Core i7-4650U FANless
Power Supply: DC
Memory: 16GB
Operating System: Windows Embedded 8.1 Industry 64 bits MUI
Storage Device Size: HDD 1TB
Optional Interfaces: No Optional Interfaces
2nd Storage: HDD 1TB
Software: Vijeo XL Runtime 64K License Key code
 
 The Base Part Number of the CPU/Motherboard module is: HMIBMP0I74DI00A
http://eshop.schneider-electric.com/product.aspx?org=21&lang=1&dist=276&prod_id=HMIBMP0I74DI00A
Click on the "Download your HMIMBP0I74DI00A datasheet" link near the top to generate a PDF.
 
The product part number for the Display is:  HMIDMA521
https://www.se.com/ww/en/product/HMIDMA521/display-pc-wide-22%27%27-multi-touch-for-hmibm/?range=61054-magelis&node=684640674-box%2C-rack-%26-display
 
 
Note:
The code HMIPCCP2NM7DA8K0KL00 is a configured variant of the HMIBMP0I74DI00A with two notable differences:
1) The HMIBMP0I74DI00A does not come with a selected Storage Harddrive, whereas the HMIPCCP2NM7DA8K0KL00  adds a 1TB HDD (magnetic).
2) The HMIBMP0I74DI00A does not come with a Vijeo XL License (EcoStruxure Machine SCADA Expert), whereas the HMIPCCP2NM7DA8K0KL00 adds a Vijeo XL 64K License (which can also be purchased separately)
 
Other variants of the Modular Box PC HMIBM Performance can be considered as well from the catalog:
http://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=DIA5ED2140501EN.pdf&p_Doc_Ref=DIA5ED2140501EN
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.