Can I issue a command to a drive from a communication network that will cause it to save its program into the attached keypad?
Published date:
13 November 2018
Issue:
Customer is an OEM that is trying to automate their process to program our drives in their equipment. They want to use a PLC to program the drive and then issue a command from the PLC that will cause the drive to save a backup copy of its program into the attached keypad.
Product Line:
All Altivar products.
Environment:
All models, All serial numbers.
Cause:
No instructions available for this feature.
Resolution:
This is not possible on any drive via any serial communication network. For the drives that have the feature allowing a backup copy of the program to be stored in the attached keypad, the command to initiate the save function must be triggered manually from the keypad itself.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.