Browse FAQs

Can the two Ethernet ports on the HMIG5U2 be used on a dual level ring (DLR)?

Published date: 15 November 2018

Issue:
The HMIG5U2 does not support DLR.  

Product Line:
HMIG5U, HMIG5U2

Resolution:
The two Ethernet ports on the HMIG5U2 is to separate the IT/ corporate with the automation network or to connect to devices on different network.
One possible solution is using the DLR TAP. (Belden RED25 managed switch series) 
https://se--c.na72.content.force.com/servlet/servlet.FileDownload?file=00P1H000019qzCB


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.