Browse FAQs

Video: Can I use the ISO file if I can't burn/mount a DVD?

Published date: 10 February 2020

Issue
Having a problem trying to burn or mount the ISO file.

Product line
Unity, Vijeo Designer, SoMachine, any ISO file.

Resolution
It is not necessary to either burn a disk or mount the ISO file. Simply use 7Zip and extract the file to the hard drive much in the same way a ZIP file would be extracted. After extraction, install by running the appropriate setup file.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.