Browse FAQs

How to configure ION9000 basic settings using the web interface?

Published date: 14 March 2019

Issue
A user may require configuring ION9000 basic settings using its web interface.
 
Product line
ION9000
 
Environment
ION9000

Cause
Users can configure/view ION9000 basic settings using the meter's web interface.
 
Resolution
Using a browser:
  1. Type in the meter's IP address in the address bar and hit Enter.
  2. In ION9000 Login Page type the meter username and password (the default username and password are 9000 and 0, respectively).
  3. Navigate to the Setup tab.
  4. Click on the metering menu.
  5.  From here you will be able to navigate to the appropriate menus for Basic and Advanced Settings configuration.
 
Basic settings menu


Advanced Settings menu

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.