What type of load and torque-speed curve is created by screw compressor?
Published date:
13 December 2018
Dependance between the torque and speed in screw compressor is constant in general. Exact shape of torque-speed curve can vary by screw compressor type and manufacturer.
Starting torque in screw compressor is very often achieves rated torque, therefore selection of the drive must be done in the same way as for constant torque applications.
ATV900 or ATV71 series.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.