Browse FAQs

ClearSCADA: ViewX upgrade in ClearSCADA 2017

Published date: 28 December 2018

Below are the steps to install or upgrade ViewX only in ClearSCADA 2017.  These steps would typically be followed when installing/upgrading ViewX on a remote PC.


Run the installer and select 'Install ClearSCADA'.





Follow the Wizard until it presents you with three choices: Full, Typical & Custom.  Choose the 'Custom' option.





In order to run ViewX on a remote PC you must install the following modules:
  • ViewX client
  • Data Access
  • Server Management Utilities





Finish running through the Wizard to complete the ViewX installation.

Once ViewX is installed you will need to license it.  The licensing of ViewX is covered in Knowledge Base article FA299727 - Server and Client Licenses in ClearSCADA

https://www.se.com/ca/en/faqs/FA299727/
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.