Browse FAQs

Osisense XC - Picture of the cable entry adaptor DE9RA1012

Published date: 21 January 2019

Attached picture of the cable entry adaptor DE9RA1012 from Pg 11 to 1/2" NPT, metallic. It can be associated to the following limit or safety switch series using Pg 11 cable entry for example : basic XCNT, XCNTR, XCKM, XCSTE, XCSTA. The adaptor is supplied with a nut on the threaded part.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.