Issue: Can I use existing unused components in the SFLEX212 to configure it for a bypass functionality?
Product Line: ALTIVAR 212
Environment: SFLEX212 SFD212
Cause: SFD212xx was ordered without bypass.
Resolution: There are no recommendations to modify or field install a bypass functionality with existing unused components in an SFD212xx ordered without bypass.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.