Browse FAQs

Can other language be used in Varplus logic VPL12 ?

Published date: 04 February 2019

NO, it is not possible.
Display does not represents matrix. On the contrary, some texts and symbols are imprinted in the display, so they cannot be modified, then only can be switched on or off. For example texts INFO, MANUAL, SETUP, AUTO, ALARM, EXPORT, cos, THD, PQSUI, VAWvarh, FAN
The rest part of display contains 3 in upper row and 4 , 7-segment digits/characters in lower row.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.