{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Removing Control Expert and installing Unity Pro.
Remove Control Expert either through the Control Panel - Program and  Features or
Start - Programs - EcoStruxure Control Expert - Control Expert - Remove Control Expert and Run as Administrator.
Reboot the PC.

In addition, the following folders must be manually removed when replacing Control Expert with a Unity Pro Version

Once Control Expert is removed, delete the following:

- Windows 7 (32 bits):
- C:\Program Files\Common Files\Schneider Electric Shared\Tlb
- C:\Program Files\Common Files\Schneider Electric Shared\Common
- C:\Program Files\Common Files\Schneider Electric Shared\SRCSDK
- C:\Program Files\Common Files\Schneider Electric Shared\SSTA

- Windows 7 (64 bits):
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\Tlb
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\Common
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\SSTA

Schneider Electric Global