Why are the panel cut out tolerances so tight (+1mm / - 0mm) on the HMIGTO?
Published date:
07 February 2019
Issue: Why are the panel cut out tolerances so tight (+1mm / -0 mm) on the HMIGTO?
Product Line: HMIGTO series (all models)
Resolution: The panel cut out tolerances are so tight (+1 mm / - 0 mm) for the HMIGTO in order to achieve IP65 rating. It is necessary to be precise when IP65 rating is required.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.