Is there a function block in Unity Pro to compare REAL data types similar to the COMPARE block that compare INT data type?
Published date:
08 February 2019
No. There is no function block in the standard library to compare REAL data type variables similar to the COMPARE block. Attached is a DFB that compare REAL data type variables.