Browse FAQs

Can we add aux contact to vario switch used in ATV650D30N4?

Published date: 18 February 2019

Yes, it is possible.
ATV650, size B (30kW-45kW) has free space on the sides (42mm on left side and more than 100mm on right side).
This ATV size has Vario V5 inside, use aux. block compatible with V5 body. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.