{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can an ATV320 SoMove file be converted from a 3HP to a 7.5HP unit?

Issue:
User is replacing an existing motor where the installed drive is ATV320, 3HP and the new motor will be 7.5HP.  They want to keep the same programming and communication addressing and setup.  They have the SoMove files for the existing drive.

Product line:
Altivar 320, ATV320 Machine drive

Environment:
SoMove

Cause:
Change of motor size

Resolution:
Yes, you can change the part number or accessories used in the drive (i.e. option cards) using SoMove to maintain the same program settings but change the drive size.

*Note - make sure you are not connected to the drive.

Open the saved SoMove file.  At the top menu, open the Device menu.  Select Edit Topology.
A new window opens for you to select a new Reference (part number).
Once a new number is selected a warning message comes up that a partial factory reset is completed.  Click OK to continue.
Click OK on the selection window.

You can now save the new settings and load into the drive.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Global

Attachment(s)
Device - Edit Topology.JPG.jpg [19.98 KB]
Device - Edit Topology Partial Factory.JPG.jpg [26.42 KB]