Preventa XCS - How to order the XCSZP7002 or XCSZP7005 part number?
Published date:
24 June 2019
Find attached the picture of both part XCSZP1 magnet and XCSZP7002 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMP7002, having a 2m length cable. XCSZP7005 has a cable of 5m length and this complete set can be ordered with the reference XCSDMP7005
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.