How do I connect to a SoMachine controller though EcoStruxure Secure Connect Advisor?
Published date:
05 March 2019
Issue:
The EcoStruxure Secure Connect Advisor allows to connect to the controller remotely through a VPN connection.
Product Line:
M241
M251
LMC058
Environment:
SoMachine V4.3
Resolution:
1) Establish the VPN connection with EcoStruxure Secure Connect Advisor.
2) Test the connecting with a Ping command to the PLC.
4) Double click on the controller under the device tree. Under the Controller selection select IP Address via NAT (Remote TCP)
5) Enter the IPaddress of the PLC under NAT Address and Target IP address. The port is usually 1105.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.