Browse FAQs

Can I use a Vijeo Designer recipe object from the Webgate ?

Published date: 22 May 2019

Issue:
There are certain limitations while using Recipe objects in Web Gate.

Product Line:
XBTGT
HMIGTO
HMIGTU
IPC with VJD Runtime

Environment:
Vijeo Designer V6.2

Resolution:
The Data Sharing for the recipe control variable (_RecipeControlDefault) must be set to None. 
Also the Internal Recipe variables associated to the ingredients must be set to none.
The external Recipe variables associated to the ingredients can be set to Read/Write.





 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.