Browse FAQs

What are the S-flex enclosed drives minimum side by side spacing recommendations?

Published date: 07 March 2019

Issue:
What is the minimum mounting spacing recommendation when installing the S-Flex enclosed drives?

Product Line:
S-flex enclosed Drives Nema 1

Environment:
All 

Cause:
Mounting clearance 

Resolution:
Mount each device so that the door can be opened at least 90°. The following are spacing recommendations:

• Mount all units with a minimum of 6.0 in. (152 mm) of space to the top and
bottom.

• Mount 1–40 hp 208/230 V and 1–60 hp 460 V units with a minimum of 3.5 in.
(89 mm) of space to the left and right.

• Mount 75–100 hp 460 V units with a minimum of 4.0 in. (102 mm) of space to
the left and right.

https://www.se.com/us/en/download/document/30072-451-83/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.