Browse FAQs

What is the NSYAEFPFPTD accessory to the NSYPTDS* flange kit?

Published date: 09 March 2019

Issue:
What is the NSYAEFPFPTD accessory to the NSYPTDS* flange kit?

Product Line:
Process drives

Environment:
NA

Cause:
Option or required?

Resolution: 
When a Process drive is flange mounted into a wall mounted enclosure, the heatsink extends out the back.  Space is required between the enclosure and wall to accommodate the heatsink and airflow.  The NSYAEFPFPTD is a bracket kit to extend the enclosure away from the wall.  The bracket can provide the space for the NSYPTDS1, NSYPTDS2, and NSYPTDS3 flanged drives.
See the attached file.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.