Browse FAQs

What wire gage is needed for the Advantys power supplies for PE (protective earth)

Published date: 05 November 2019

Issue:
Wire size for grounding to protective earth for the Advantys power supplys.

Product Line:
Advantys

Resolution:
PE is brought to the island by a heavy-duty cross-sectional wire, usually a copper braided cable, 4.2 mm2 (10 gage) or larger. The wire needs to be tied to a single grounding point. The ground conductor connects to the bottom of the each PDM base and is secured by the PE captive screw.
Note: Local electrical codes take precedence over our PE wiring recommendations. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.