Browse FAQs

Osisense XC - Difference between both variable length dia50mm roller levers ZCY49 and ZCY69

Published date: 22 March 2019

The difference between both variable length dia50mm roller levers ZCY49 and ZCY69 is the track of the roller. It is fixed in the ZCY49 roller lever (40mm) and adjustable in the ZCY69 roller lever (from 50 to 72mm). Attached picture of the ZCY69 special dia 50mm roller lever.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.