Browse FAQs

The Magelis XBTGTW652 12in Advanced Open Touchscreen Panel is out of production. What is its replacement?

Published date: 29 March 2019

Issue
The Magelis XBTGTW652 12" Advanced Open Touchscreen Panel is out of production. What is its replacement?

Product Line
Magelis iPC

Environment
Physical HMI

Resolution
The recommended replacement for the XBTGTW652 is the Magelis HMIG5U2 Open BOX with HMIDT642 12.1" Touch Smart Display (XGA).
These two parts snap together to form one mountable HMI unit with the same cutout dimensions as the original XBTGTW652.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.