Browse FAQs

Preventa XY2C - Is it permissible to replace the contact block in XY2CH E.stop rope pull switches

Published date: 12 June 2019

Telemecanique Sensors does not allow to replace contacts in the safety components red painting like XCS safety switches, XY2C E.stop rope pull switches, ... They are not sold in spare parts. For the XY2CH switches, the contact bloc is fixed by a one-way screw, meaning it is not replaceable. Another restraint is the fact that the 2-contact block XE2NP** is special and it is not sold in spare parts. Please see attached picture. Note there is a warning into the instruction sheet to prohibit such operation (see attachment). It is the same situation for the other rope pull switches XY2CE, XY2CED & XY2CJ. For these products a red varnish is applied on the one-way screws.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.