{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to enable Product Restart via communication for Altivar ATV variable speed drives
There are 2 parameters for product restart.
One is RP. If value 1 is written to RP, the product will restart. In this way product restart can be activated via HMI as well. RP has logic address 16#1BD8 = 7128
Second method is to assign a logic input or a bit written via communication. Assignment can be done via HMI. Somove or communication. See attached table with the possible RPA assignment.
For example if you assign RPA= CD11, the product restart can be activated by bit 11 in CMD word sent by active control channel.

Schneider Electric Global

Attachment(s)
RP, RPA.txt [4.01 KB]