Browse FAQs

Preventa XCS - Behaviour of the XCSRC RFID contactless safety switch, standalone model with monitored restart button, if the restart is actuated when the guard is open

Published date: 03 May 2019

Q) Does the switch fail in error when the “magnet” or transponder is not closed to the reader and that the restart button is activated? See attached diagram
A) Test did on a sample: nothing happens, no switch error, the switch or reader is waiting for the transponder before starting the EDM loop test. Only the green del TR lights, the second led RD is off.
In the normal conditions, transponder present, the TR led is green, the RD led is blinking in orange color. Explanation, the switch is waiting for the start command. After start, the led becomes green, if the start conditions are closed

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.