{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the ATV340 keypad (VW3A1113) have its own mounting kit?
Issue:
What is the part number of the mounting kit for the ATV340 keypad (VW3A1113)?

Product Line:
Altivar Drives

Environment:
Open style drive

Cause:
Mounting kit for VW3A1113

Resolution:
Frame sizes 1-3 have the ability to mount the VW3A1113 directly on the front of the drive.
VW3A1114 is the part number for the keypad mounting kit..

Keypad mounting kit

The Altivar 340 drive can also use the Graphic Display Terminal VW3A1111 (also used on the Altivar Process Drives), which can be connected to the drive using the Remote mount kit (VW3A1112) and a Modbus cable.

Frame sizes 4 and 5 allow mounting of the VW3A1111 display directly on the front of the drive.

NOTE: The drive does not come with either of these displays.  They must be ordered separately.

Schneider Electric Global

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: