Browse FAQs

How can the BMEP58_ECPU_EXT.NETWORK_HEALTH DDT be reset?

Published date: 22 May 2019

Issue
After correcting a network topology or broadcast storm issue, the network health bit did not reset.

Product line
Control Expert, Unity Pro, M580

Resolution
Before firmware version 2.80, a power cycle of the CPU was required to reset the bit. From V2.80 forward, the bit will reset itself after the problem is corrected. A firmware upgrade is recommend to correct the behavior.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.