Browse FAQs

How to get PRM Master 1.1.4.0?

Published date: 19 November 2020

Issue
The latest version of PRM 1.2 ISO has the PRM Master DTM is 1.1.3.0, but some projects show the PRM Master DTM as version 1.1.4.0 and the project doesn't build with this discrepance

Product Line
Unity Pro, Control Expert, PRM, TCSEGPA23F14F   

Environment
Control Expert v14, Unity Pro v13.1 

Resolution
On the PRM 1.2 .ISO, you need to launch the index.hta to install a Patch for Master DTM (7-Krohne\MasterDTM\PRMmasterDTMPatch.exe) this patch changes the version of PRM Master from 1.1.3.0 to 1.1.4.0.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.