{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?
Issue:
A customer asks if the 800mm wide NetShelter cabinet has a larger cable management capacity.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
A customer is trying to choose 750mm vs. 800mm wide cabinets.

Resolution:

The 750mm wide and 800mm wide cabinets use the same vertical cable managers so they have the same cable management capacity.
For example; AR7580A is the high volume vertical cable manager used in AR3150 and AR3350, and also in AR3180G and AR3380G.

Schneider Electric Global