Browse FAQs

Preventa XY2C - Picture of the rope pull switch XY2CE1D296 having a cable tension viewing window for adjustment when the cover is closed

Published date: 03 June 2019

Find attached the picture of the E.stop rope pull switch XY2CE1D296 having a cable tension viewing window for adjustment when the cover is closed and a LED, 24 - 130 V supply voltage pilot light. Such reference is available to order in 2019, such as the following ones : XY2CE1D297 with LED, 230 V supply voltage pilot light, XY2CE2D296 and XY2CE2D297

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.