{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Why doesn't SoMove Software show all assigned inputs under the Operate Tab, Input/Output terminals?

Issue:
Why doesn't SoMove Software show all assigned inputs under the Operate Tab, Input/Output terminals?

Product Line:
Altivar Machines, SoMove Software

Environment:
All models and serial numbers

Cause:
Programming

Resolution:
Per Level 3 - There is a limitation on SoMove, we see only LI1 and LI2 logic input, no LI3 to LI6.
The limitation is to avoid SoMove Modbus overload which can cause SoMove untimely disconnection.

Did this answer your question?

Explore more
Range:
SoMove
Explore more
Range:
SoMove
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.