Browse FAQs

Which Unity Quantum CPUs support both the 140CRP31200 and 140CRP93x00 in the local CPU rack?

Published date: 05 July 2019

Issue: 
Which Unity Quantum CPUs support both the 140CRP31200 and 140CRP93x00 in the local CPU rack


Product Line:
Unity Pro, Quantum, 140CRP31200, 140CRP93x00


Resolution:
Only the Quantum 140CPU658-60, 140CPU672-61 and 140CPU678-61 will support both CRP modules on the local rack

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.